Close
Filters
Search
RSS

Blog

Keeping a ZEBRA® in your toolbox!

If you only know zebras from the zoo, you've missed something for decades! Because ZEBRA® is the quality brand from Würth that impresses with innovation, durability and the promise of guarantee. And for these reasons, you should quickly make room for ZEBRA® in your tool box.

The high quality standard makes a difference!

Good tools are durable and can ideally be used for many years. The ZEBRA® brand at Würth has stood for the highest perfection and quality for over 40 years. ZEBRA® products are subject to the strictest quality tests. In our in-house quality assurance they are tested under extreme conditions and achieve top values. Before the market launch, engineers, technicians and foremen subject all new products to rigorous practical tests.

Products from the current range are also constantly checked and optimized. This is the only way to guarantee the highest quality. Thanks to accreditation according to DIN EN ISO / IEC 17025, the Würth test laboratory is able to ensure product testing in a competent and independent manner.

You will no longer use any other tool!

There is a 100% promise of satisfaction on all ZEBRA® products. Screwdrivers , ratchets, pliers - if you are not satisfied with a ZEBRA® tool or it breaks, even though it has been used properly, put it on the table in the nearest customer center and you will get a new one. Very easy, and even after many years!

Protecting your most important tool!

The hands are the most direct tool of man. Almost nothing works without them. How much we depend on them is usually determined when there is an injury.A small cut in the fingertip is enough to spoil us for a whole working day, a pinched finger occupies us for weeks. Every craftsman pays attention to his tools. It not only protects it from gross damage, but also ensures proper care.

The following therefore applies to our hands:

  • Skin protection before starting work. Modern skin protection creams form a thin protective film over the skin, thus preventing the penetration of microparticles, drying out and the formation of allergies.
  • Skin cleaning after dirty work. Up-to-date soaps can be expected to quickly remove the dirt particles from the skin (too long rubbing damages the superficial skin cells), but not to upset the skin's PH value too much. Try our cleaning product for effective cleaning after a hard day's work.
  • Skin care after work. To promote skin regeneration after a hard day's work. The skin needs moisturizing support such as  lotions  , especially in the cold season .

Therefore, pay attention to high-quality skin protection and skin care products, hand cleaners, foams, lotions and work gloves for your areas of application. Professional skin protection, skin cleaning and skin care on the most important tool of human beings, our hands, pay off!

Why good tools have a price!

Longevity & Guarantee

Good tools are durable and can ideally be used for many years. The ZEBRA® brand at Würth has stood for the highest perfection and quality for over 40 years. Therefore, there is a 100% promise of satisfaction on ZEBRA® products.

Ergonomics

A tool should definitely be in your hand. And that is also a good indicator that you can work with it for a long time without fatigue. Good handling is not only particularly important, for example with pliers. The combination plier with the ergonomic and non-slip 2-component comfort grip with slim collar shape ensure comfortable working and optimal power transmission.

Additional Benefits

There are tools that can do more. This is an important criterion for professionals when choosing tools. Do you know a " dust-free ratchet "? This offers protection against dirt as it is closed and therefore neither dust nor dirt can get in, which means that the mechanics remain permanently lubricated and negative environmental influences do not affect the moving parts: the ratchet is completely maintenance-free!

Not sure which tool to choose for your daily work? Get advice from experts by contact Wurth Malta today!

Zebra logo

Drilling with the best Tools
Drilling with the best Tools

Drilling is one of the most common jobs in the craft. To prevent blunt drills or frayed drill holes, you can do the following: choose the winner among the HSCO drills , the spiral drill from Würth.

You probably know this when you start the drill, switch on the drill and the tip of the drill slips off. Or if the drill gets stuck. Or if you need a whole arsenal of different drills to always have a suitable one for your needs. These problems are time-consuming and nerve-racking and, above all, unprofitable.

High quality HSCO drills according to DIN 338 in different qualities are used every day . These drills are characterized above all by high tempering resistance, wear resistance and heat hardness. Choosing a high-quality drill that can withstand everyday stresses guarantees precise work.

What is the difference between the Würth HSCO DIN 338 MFC Speed ​​drill and other drills? Quite simply, he is the winner among the drills. What that means? It wins countless tests and is very popular because it solves many problems that arise during drilling.

It enables optimal centering, even on curved surfaces. And as the name “Speed” suggests in the name, it is the fastest among the drills. Thanks to the new speed geometry of the drill, you can get to your drill holes up to 50% faster than with conventional, ground twist drills.

It ensures precise drilling with hand-held use in almost all materials, such as stainless steel (e.g. V2A, V4A), heat-resistant steels, conventional steel up to 1,200 N / mm² strength, cast iron, non-ferrous metals (e.g. aluminum, aluminum alloys, bronze, plastic) and also titanium.

The Würth high-speed drill is truly an all-rounder and solves frequently occurring problems that arise during drilling. You save time and trouble and are well equipped.

For more information about this drill bit you can watch the following clip. 

Piece adapted from Wurth Austria Online Magazine

Wurth Mud Flaps
Wurth Mud Flaps

If you are set on the awesome look of metal flaps, you should realize that they are better suited for soft dirt, sand or wet mud. This is where the how you use your truck application comes in. For the best mud flaps, please visit our Wurth Mud Flaps. They are durable, are of high quality and are the best options for your vehicle.

https://eshop.wuerth.com.mt/mud-flaps

Safety Shoes - Protection at Work
Safety Shoes - Protection at Work

When we speak about industrial safety shoes, it is usually the heavy duty footwear that comes to your mind such as the steel toe boots. The thing with these boots is that they have reinforced toes that tend to protect your feet from the hazards like heavy objects found at construction and industries worksites.

It is not just the steep toe boots but there are different types of shoes exist that can make the jobs safer.  So, how do these safety shoes keep you protected at the workplace? Let’s find out.

Foot injuries are usually debilitating. They can keep you away from work or cause difficulty in performing a job at hand. These are ways in which Wurth's safety shoes can protect you from injury at work.

PROTECT FROM FALLING & FLYING OBJECTS

When the workers carry heavy materials in the workplace where there are several vehicles or machineries, flying and falling objects are a common thing. Protective shoes from brands like Wurth S3 can be a life saver.

PROTECT FROM PUNCTURES 

At workplace, there might be a time when you step on some sharp object or get stuck by sharp object from above. Shoes with thick materials and heavy duty sole like ones from brands like Wurth S2 offer the best protection to your feet.

PROTECT FROM CUTTING HAZARDS

Sharp machineries or the ones that contain moving parts might lead to several cutting hazards. For instance, workers who work in the wood industry experience dangers from the chain saws. 

PROTECT FROM ELECTRICAL HAZARDS

Electricity again has its own share of hazards at the workplace. Workplace might experience electric shocks or accumulate static electricity that can lead to electric sparks in the industry. In order to reduce the risk of an electrical accident, you must wear non-conductive footwear made from rubber, leather or other materials.

PREVENT SLIPS, TRIPS & FALLS

Falls, trips and slips can happen in just about every workplace. Industries must therefore take due measures to install anti slip floor tape in order to reduce the risk of mishaps. Proper safety shoes can also do the needful and keep you protected from these slips and falls.

PREVENT FATIGUE

For workers who stand all day especially on the hard surfaces such as concrete, fatigue can be a big problem. Muscles of the feet as well as the legs, back and the other parts of the body tend to feel tired and the situation can be aggravated if the employees don’t wear the right type of footwear. SoFree Web Content, look for shoes that are more comfortable and offer the requisite cushioning.

You can buy these safety shoes online. Safety shoes online shopping can be convenient and time and money saving. 

Article abridged from the Article Factory. 

Close